TableCollection Class¶
-
class
NXOpen.Diagramming.Tables.
TableCollection
¶ Bases:
object
Represents a collection of Table.
To obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateTableBuilder | Creates a NXOpen.Diagramming.Tables.TableBuilder . |
FindObject | Finds the NXOpen.Diagramming.Tables.Table with the given identifier as recorded in a journal. |
Method Detail¶
CreateTableBuilder¶
-
TableCollection.
CreateTableBuilder
¶ Creates a
NXOpen.Diagramming.Tables.TableBuilder
.Signature
CreateTableBuilder(table)
Parameters: table ( NXOpen.Diagramming.Tables.Table
) –NXOpen.Diagramming.Tables.Table
to be edited, if None then create a new oneReturns: Return type: NXOpen.Diagramming.Tables.TableBuilder
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
TableCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.Tables.Table
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with given name.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: NXOpen.Diagramming.Tables.Table
with this name.Return type: NXOpen.Diagramming.Tables.Table
New in version NX10.0.0.
License requirements: None.