SheetManager Class¶
-
class
NXOpen.Diagramming.
SheetManager
¶ Bases:
object
A manager to deal with all objects.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ActiveSheet | Returns or sets the active sheet |
Methods¶
Method | Description |
---|---|
OpenSheet | Opens a NXOpen.Diagramming.Sheet . |
Property Detail¶
ActiveSheet¶
-
SheetManager.
ActiveSheet
¶ Returns or sets the active sheet
-------------------------------------
Getter Method
Signature
ActiveSheet
Returns: Return type: NXOpen.Diagramming.Sheet
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSheet
Parameters: sheet ( NXOpen.Diagramming.Sheet
) –New in version NX12.0.0.
License requirements: None.
Method Detail¶
OpenSheet¶
-
SheetManager.
OpenSheet
¶ Opens a
NXOpen.Diagramming.Sheet
.Signature
OpenSheet(sheet)
Parameters: sheet ( NXOpen.Diagramming.Sheet
) –New in version NX12.0.0.
License requirements: None.