SheetElementBuilderResizeOptionType Enumeration

NXOpen.Diagramming.SheetElementBuilder.ResizeOptionType is an alias for NXOpen.Diagramming.SheetElementBuilderResizeOptionType

class NXOpen.Diagramming.SheetElementBuilderResizeOptionType

Bases: object

Represents the resize option for a NXOpen.Diagramming.SheetElementBuilder.

New in version NX11.0.0.

Enum Members

Enum Member Enum Member Description
AnyDirection
OnAnchor
SameRatio
SameRationOnCorner
SameRatioOnEdge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.