SheetCollection Class¶
-
class
NXOpen.Diagramming.
SheetCollection
¶ Bases:
object
Represents a collection of Sheet.
To obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateSheetBuilder | Creates a NXOpen.Diagramming.SheetBuilder . |
FindObject | Finds the NXOpen.Diagramming.Sheet with the given identifier as recorded in a journal. |
Method Detail¶
CreateSheetBuilder¶
-
SheetCollection.
CreateSheetBuilder
¶ Creates a
NXOpen.Diagramming.SheetBuilder
.Signature
CreateSheetBuilder(sheet)
Parameters: sheet ( NXOpen.Diagramming.Sheet
) –NXOpen.Diagramming.Sheet
to be edited, if None then create a new oneReturns: Return type: NXOpen.Diagramming.SheetBuilder
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
SheetCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.Sheet
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with given name.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: NXOpen.Diagramming.Sheet
with this name.Return type: NXOpen.Diagramming.Sheet
New in version NX10.0.0.
License requirements: None.