ShapeBuilder Class

class NXOpen.Diagramming.ShapeBuilder

Bases: NXOpen.Diagramming.SheetElementBuilder

Represents a ShapeBuilder.

To create a new instance of this class, use NXOpen.Diagramming.ShapeCollection.CreateShapeBuilder()

New in version NX10.0.0.

Properties

Property Description
Height Returns or sets the height.
HeightPolicy Returns or sets the height policy.
Internal Returns the flag that indicates if the sheet element is internal.
Label Returns the label of this sheet element.
LabelName Returns or sets the label name of this sheet element.
Location Returns the location of the sheet element relative to another sheet element.
LocationStyle Returns or sets the location style.
MirrorX Returns or sets the sheet element to Mirror along the X axis.
MirrorY Returns or sets the sheet element to Mirror along the Y axis.
Owner Returns or sets the owning sheet element.
OwningSheet Returns the owning sheet.
ResizeOption Returns or sets the resize option of the sheet element
Rotation Returns or sets the rotation angle that is counter clockwise and relative to the owner.
SourceElement Returns the source element that records which sheet element it is a copy of.
Tag Returns the Tag for this object.
UpToDate Returns the flag that indicates if the sheet element is up to date.
Visible Returns the flag that indicates if the sheet element is visible.
Width Returns or sets the width.
WidthPolicy Returns or sets the width policy.
NXOpen.Diagramming.SheetElementBuilder.X Returns or sets the absolute x coordinate.
NXOpen.Diagramming.SheetElementBuilder.Y Returns or sets the absolute y coordinate.
ZDepth Returns or sets the Z depth.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetAllowedTransformations Get the allowed transformations of the sheet element.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetMinNodeSize Gets the minimum node size values
GetObject Returns the object currently being edited by this builder.
SetMinNodeSize Sets the minimum node size values
SetOwningSheet Set the owning sheet when the sheet element is created.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

ShapeBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.