NodeCollection Class

class NXOpen.Diagramming.NodeCollection

Bases: object

Represents a collection of Node.

To obtain an instance of this class, refer to NXOpen.Diagramming.DiagrammingManager

New in version NX10.0.0.

Methods

Method Description
CreateNodeBuilder Creates a NXOpen.Diagramming.NodeBuilder.
FindObject Finds the NXOpen.Diagramming.Node with the given identifier as recorded in a journal.

Method Detail

CreateNodeBuilder

NodeCollection.CreateNodeBuilder

Creates a NXOpen.Diagramming.NodeBuilder.

Signature CreateNodeBuilder(node)

Parameters:node (NXOpen.Diagramming.Node) – NXOpen.Diagramming.Node to be edited, if None then create a new one
Returns:
Return type:NXOpen.Diagramming.NodeBuilder

New in version NX10.0.0.

License requirements: None.

FindObject

NodeCollection.FindObject

Finds the NXOpen.Diagramming.Node with the given identifier as recorded in a journal.

An exception will be thrown if no object can be found with given name.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier to be found
Returns:NXOpen.Diagramming.Node with this name.
Return type:NXOpen.Diagramming.Node

New in version NX10.0.0.

License requirements: None.