LeaderLineBuilderVerticalAlignmentOption Enumeration¶
NXOpen.Diagramming.LeaderLineBuilder.VerticalAlignmentOption is an alias for NXOpen.Diagramming.LeaderLineBuilderVerticalAlignmentOption
-
class
NXOpen.Diagramming.
LeaderLineBuilderVerticalAlignmentOption
¶ Bases:
object
Represents the option
NXOpen.Diagramming.LeaderLineBuilder.VerticalAlignment()
for aNXOpen.Diagramming.LeaderLineBuilder
.New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description Top Setting the vertical alignment top Middle Setting the vertical alignment middle Bottom Setting the vertical alignment bottom -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-