DiagrammingArrowtype Enumeration¶
-
class
NXOpen.Diagramming.
DiagrammingArrowtype
¶ Bases:
object
Represents the arrow type.
New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description NotSet Setting the arrow type none arrow Open Setting the arrow type open arrow Filled Setting the arrow type filled arrow ClosedSolid Setting the arrow type closed solid arrow -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-