AnnotationBuilder Class¶
-
class
NXOpen.Diagramming.
AnnotationBuilder
¶ Bases:
NXOpen.Diagramming.ConnectableElementBuilder
Represents a AnnotationBuilder.
To create a new instance of this class, use
NXOpen.Diagramming.AnnotationCollection.CreateAnnotationBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BoundaryDisplay | Returns or sets the visibility of boundary. |
BoundaryType | Returns or sets the boundary type of the annotation |
FormattedStringBuilder | Returns the formatted string of the text. |
Height | Returns or sets the height. |
HeightPolicy | Returns or sets the height policy. |
Internal | Returns the flag that indicates if the sheet element is internal. |
Label | Returns the label of this sheet element. |
LabelName | Returns or sets the label name of this sheet element. |
Location | Returns the location of the sheet element relative to another sheet element. |
LocationStyle | Returns or sets the location style. |
MirrorX | Returns or sets the sheet element to Mirror along the X axis. |
MirrorY | Returns or sets the sheet element to Mirror along the Y axis. |
Owner | Returns or sets the owning sheet element. |
OwningSheet | Returns the owning sheet. |
ResizeOption | Returns or sets the resize option of the sheet element |
Rotation | Returns or sets the rotation angle that is counter clockwise and relative to the owner. |
SourceElement | Returns the source element that records which sheet element it is a copy of. |
Tag | Returns the Tag for this object. |
Text | Returns or sets the text should be used only when textType is Diagramming. |
TextStyleBuilder | Returns the text style of the annotation. |
TextType | Returns or sets the text type. |
UpToDate | Returns the flag that indicates if the sheet element is up to date. |
Visible | Returns the flag that indicates if the sheet element is visible. |
Width | Returns or sets the width. |
WidthPolicy | Returns or sets the width policy. |
NXOpen.Diagramming.SheetElementBuilder.X | Returns or sets the absolute x coordinate. |
NXOpen.Diagramming.SheetElementBuilder.Y | Returns or sets the absolute y coordinate. |
ZDepth | Returns or sets the Z depth. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllPorts | Gets all ports of this connectable element. |
GetAllowedTransformations | Get the allowed transformations of the sheet element. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMinNodeSize | Gets the minimum node size values |
GetObject | Returns the object currently being edited by this builder. |
GetPorts | Gets ports of this connectable element by the direction. |
SetMinNodeSize | Sets the minimum node size values |
SetOwningSheet | Set the owning sheet when the sheet element is created. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AnnotationBuilderTextTypeOption Enumeration | Represents the option NXOpen.Diagramming.AnnotationBuilder.TextType() for a NXOpen.Diagramming.AnnotationBuilder . |
Property Detail¶
BoundaryDisplay¶
-
AnnotationBuilder.
BoundaryDisplay
¶ Returns or sets the visibility of boundary.
If return true, the annotation will show its boundary if it has one.
-------------------------------------
Getter Method
Signature
BoundaryDisplay
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryDisplay
Parameters: boundaryDisplay (bool) – New in version NX10.0.0.
License requirements: None.
BoundaryType¶
-
AnnotationBuilder.
BoundaryType
¶ Returns or sets the boundary type of the annotation
-------------------------------------
Getter Method
Signature
BoundaryType
Returns: Return type: NXOpen.Diagramming.DiagrammingAnnotationboundarytype
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryType
Parameters: boundaryType ( NXOpen.Diagramming.DiagrammingAnnotationboundarytype
) –New in version NX10.0.0.
License requirements: None.
FormattedStringBuilder¶
-
AnnotationBuilder.
FormattedStringBuilder
¶ Returns the formatted string of the text.
-------------------------------------
Getter Method
Signature
FormattedStringBuilder
Returns: Return type: NXOpen.Diagramming.FormattedStringBuilder
New in version NX10.0.0.
License requirements: None.
Text¶
-
AnnotationBuilder.
Text
¶ Returns or sets the text should be used only when textType is Diagramming.
AnnotationBuilder.TextTypeOption.Fixed
-------------------------------------
Getter Method
Signature
Text
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Text
Parameters: strValue (str) – New in version NX10.0.0.
License requirements: None.
TextStyleBuilder¶
-
AnnotationBuilder.
TextStyleBuilder
¶ Returns the text style of the annotation.
-------------------------------------
Getter Method
Signature
TextStyleBuilder
Returns: Return type: NXOpen.Diagramming.TextStyleBuilder
New in version NX11.0.0.
License requirements: None.
TextType¶
-
AnnotationBuilder.
TextType
¶ Returns or sets the text type.
If
NXOpen.Diagramming.AnnotationBuilderTextTypeOption.Fixed
, the text of annotation is stored inNXOpen.Diagramming.AnnotationBuilder
. IfNXOpen.Diagramming.AnnotationBuilderTextTypeOption.Parametric
, the text of annotation is stored inNXOpen.Diagramming.AnnotationBuilder.FormattedStringBuilder()
.-------------------------------------
Getter Method
Signature
TextType
Returns: Return type: NXOpen.Diagramming.AnnotationBuilderTextTypeOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextType
Parameters: textType ( NXOpen.Diagramming.AnnotationBuilderTextTypeOption
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AnnotationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.