DatumConstraintSolution Enumeration¶
NXOpen.DatumConstraint.Solution is an alias for NXOpen.DatumConstraintSolution
-
class
NXOpen.
DatumConstraintSolution
¶ Bases:
object
Specifies the alternate solution for datum axis using point on curve method
Enum Members
Enum Member Enum Member Description Undefined Tangent Normal Binormal OppositeTangent OppositeNormal OppositeBinormal Datum axis at opposite to binormal to curve Project This direction is calculated by projecting a point selected along a curve to a line, a datum axis, an edge of a solid, a planar face or a datum plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-