DMUManager Class¶
-
class
NXOpen.DMU.
DMUManager
¶ Bases:
object
Represents an object that manages DMU application specific objects and preferences.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateSnapshotCollection | Creates the NXOpen.DMU.SnapshotCollection in the part. |
GetSnapshotCollection | Returns the NXOpen.DMU.SnapshotCollection in the part. |
ResetToDesignState | Resets the changes made to the part, related to the assets which can be captured in the NXOpen.DMU.ISnapshot . |
Method Detail¶
CreateSnapshotCollection¶
-
DMUManager.
CreateSnapshotCollection
¶ Creates the
NXOpen.DMU.SnapshotCollection
in the part.At max only one instance of
NXOpen.DMU.SnapshotCollection
can be created in a part.Signature
CreateSnapshotCollection(part)
Parameters: part ( NXOpen.Part
) –Returns: Return type: NXOpen.DMU.SnapshotCollection
New in version NX12.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetSnapshotCollection¶
-
DMUManager.
GetSnapshotCollection
¶ Returns the
NXOpen.DMU.SnapshotCollection
in the part.Signature
GetSnapshotCollection(part)
Parameters: part ( NXOpen.Part
) –Returns: Return type: NXOpen.DMU.SnapshotCollection
New in version NX12.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ResetToDesignState¶
-
DMUManager.
ResetToDesignState
¶ Resets the changes made to the part, related to the assets which can be captured in the
NXOpen.DMU.ISnapshot
.Signature
ResetToDesignState(part)
Parameters: part ( NXOpen.Part
) – Part that will get reset to design stateNew in version NX12.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)