ColorWidth Class¶
-
class
NXOpen.
ColorWidth
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.ColorWidth
used byNXOpen.WidthDefinition
to define a custom width for each color.This class contains an index into the color array and a custom width value assigned to the indexed color.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Width | Returns or sets the width associated with the color |
WidthSource | Returns or sets the width entry source. |
Methods¶
Property Detail¶
Width¶
-
ColorWidth.
Width
¶ Returns or sets the width associated with the color
-------------------------------------
Getter Method
Signature
Width
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width
Parameters: width (float) – New in version NX5.0.0.
License requirements: None.
WidthSource¶
-
ColorWidth.
WidthSource
¶ Returns or sets the width entry source.
This will be -1 if this color is not a custom width, otherwise it will be a value greater than 0 to index into the color array.
-------------------------------------
Getter Method
Signature
WidthSource
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WidthSource
Parameters: widthSource (int) – New in version NX5.0.0.
License requirements: None.