CGMImporter Class¶
-
class
NXOpen.
CGMImporter
¶ Bases:
NXOpen.Importer
Used to import a CGM file into the work part.
To obtain an instance of this class use
ImportManager.CreateCgmImporter()
.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Crosshatching | Returns or sets the crosshatching flag, true if crosshatching should be done |
FileName | Returns or sets the name of the file containing the data to import. |
Tag | Returns the Tag for this object. |
UseExportSessionWidths | Returns or sets |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Crosshatching¶
-
CGMImporter.
Crosshatching
¶ Returns or sets the crosshatching flag, true if crosshatching should be done
-------------------------------------
Getter Method
Signature
Crosshatching
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Crosshatching
Parameters: crosshatching (bool) – New in version NX7.5.0.
License requirements: None.
UseExportSessionWidths¶
-
CGMImporter.
UseExportSessionWidths
¶ Returns or sets
-------------------------------------
Getter Method
Signature
UseExportSessionWidths
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseExportSessionWidths
Parameters: useCgmExportSessionWidths (bool) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CGMImporter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.