CGMBuilderSizeOption Enumeration¶
NXOpen.CGMBuilder.SizeOption is an alias for NXOpen.CGMBuilderSizeOption
-
class
NXOpen.
CGMBuilderSizeOption
¶ Bases:
object
Specifies the size option of the CGM.
Enum Members
Enum Member Enum Member Description FullScale Full Scale ScaleFactor Scale Factor, scales the CGM based on user defined scale field Dimension Dimension, uses the units along with X and Y dimensions to determine CGM size -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-