CGMBuilderImageResolutionOption Enumeration¶
NXOpen.CGMBuilder.ImageResolutionOption is an alias for NXOpen.CGMBuilderImageResolutionOption
-
class
NXOpen.
CGMBuilderImageResolutionOption
¶ Bases:
object
Specifies the image resolution when exporting a raster image
Enum Members
Enum Member Enum Member Description Draft Draft Resolution Low Low Resolution Medium Medium Resolution High High Resolution -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-