CGMBuilderActionOption Enumeration¶
NXOpen.CGMBuilder.ActionOption is an alias for NXOpen.CGMBuilderActionOption
-
class
NXOpen.
CGMBuilderActionOption
¶ Bases:
object
Specifies the action option to be used when running Teamcenter
Enum Members
Enum Member Enum Member Description CreateNew Creates a new dataset in Teamcenter OverwriteExisting Overwrites an existing dataset in Teamcenter FileBrowser Option allows for export of CGM file to local location when running Teamcenter -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-