WorkInstructionOutputBuilderPageSizeType Enumeration

NXOpen.CAM.WorkInstructionOutputBuilder.PageSizeType is an alias for NXOpen.CAM.WorkInstructionOutputBuilderPageSizeType

class NXOpen.CAM.WorkInstructionOutputBuilderPageSizeType

Bases: object

the page size type

Enum Members

Enum Member Enum Member Description
A0
A1
A2
A3
A4
B1
B2
B3
B4
B5
Executive
Folio
Legal
Letter
Tabloid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.