WedmStatusControlCiBuilder Class¶
-
class
NXOpen.CAM.
WedmStatusControlCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a WedmStatusControlCiBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
StatusControl | Returns or sets the Wedm Status Control Type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
WedmStatusControlCiBuilderStatusTypes Enumeration | Available types for status control |
Property Detail¶
StatusControl¶
-
WedmStatusControlCiBuilder.
StatusControl
¶ Returns or sets the Wedm Status Control Type
-------------------------------------
Getter Method
Signature
StatusControl
Returns: the wedm status control type Return type: NXOpen.CAM.WedmStatusControlCiBuilderStatusTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StatusControl
Parameters: statusType ( NXOpen.CAM.WedmStatusControlCiBuilderStatusTypes
) – the wedm status control typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)