TurningOperationBuilderMotionOutputOptions Enumeration¶
NXOpen.CAM.TurningOperationBuilder.MotionOutputOptions is an alias for NXOpen.CAM.TurningOperationBuilderMotionOutputOptions
-
class
NXOpen.CAM.
TurningOperationBuilderMotionOutputOptions
¶ Bases:
object
The motion output options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description LinearOnly Linear output only Circular Linear and circular motions output MachineCycle Machine cycle motions output -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-