TurnToolBuilderThicknessTypes Enumeration¶
NXOpen.CAM.TurnToolBuilder.ThicknessTypes is an alias for NXOpen.CAM.TurnToolBuilderThicknessTypes
-
class
NXOpen.CAM.
TurnToolBuilderThicknessTypes
¶ Bases:
object
the available thickness types
Enum Members
Enum Member Enum Member Description Thickness01 Thickness: 01 ThicknessT1 Thickness: T1 Thickness02 Thickness: 02 ThicknessT2 Thickness: T2 Thickness03 Thickness: 03 ThicknessT3 Thickness: T3 Thickness04 Thickness: 04 Thickness05 Thickness: 05 Thickness06 Thickness: 06 Thickness07 Thickness: 07 Thickness09 Thickness: 09 Thickness11 Thickness: 11 Thickness12 Thickness: 12 ThicknessUserDefined Thickness: User defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-