TurnToolBuilderReliefAngleTypes Enumeration¶
NXOpen.CAM.TurnToolBuilder.ReliefAngleTypes is an alias for NXOpen.CAM.TurnToolBuilderReliefAngleTypes
-
class
NXOpen.CAM.
TurnToolBuilderReliefAngleTypes
¶ Bases:
object
the available relief angle types
Enum Members
Enum Member Enum Member Description A3 Relief angle type: A (3) B5 Relief angle type: B (5) C7 Relief angle type: C (7) D15 Relief angle type: D (15) E20 Relief angle type: E (20) F25 Relief angle type: F (25) G30 Relief angle type: G (30) N0 Relief angle type: N (0) P11 Relief angle type: P (11) OOther Relief angle type: O (other) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-