TurnToolBuilderInsertShapes Enumeration¶
NXOpen.CAM.TurnToolBuilder.InsertShapes is an alias for NXOpen.CAM.TurnToolBuilderInsertShapes
-
class
NXOpen.CAM.
TurnToolBuilderInsertShapes
¶ Bases:
object
the available insert shapes
Enum Members
Enum Member Enum Member Description Parallelogram85 Insert shape: Parallelogram 85 Parallelogram82 Insert shape: Parallelogram 82 Diamond80 Insert shape: Diamond 80 Diamond100 Insert shape: Diamond 100 Diamond55 Insert shape: Diamond 55 Diamond75 Insert shape: Diamond 75 Hexagon Insert shape: Hexagon Parallelogram55 Insert shape: Parallelogram 55 Rectangle Insert shape: Rectangle Diamond86 Insert shape: Diamond 86 Octagon Insert shape: Octagon Pentagon Insert shape: Pentagon Round Insert shape: Round Square Insert shape: Square Triangle Insert shape: Triangle Diamond35 Insert shape: Diamond 35 Trigon Insert shape: Trigon User Insert shape: User defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-