TurnThreadFinishPassesBuilder Class

class NXOpen.CAM.TurnThreadFinishPassesBuilder

Bases: NXOpen.TaggedObject

Represents a TurnThreadFinishPasses Builder

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.

Methods

Method Description
Add Create a new finish passes item.
Delete Delete an existing finish passes item
Modify Modify an existing finish passes item

Method Detail

Add

TurnThreadFinishPassesBuilder.Add

Create a new finish passes item.

Add at the end of the current List.

Signature Add(numberOfPasses, increment)

Parameters:
  • numberOfPasses (int) – the number of passes
  • increment (float) – the increment

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Delete

TurnThreadFinishPassesBuilder.Delete

Delete an existing finish passes item

Signature Delete(nodeIndex)

Parameters:nodeIndex (int) – the selected entry index

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Modify

TurnThreadFinishPassesBuilder.Modify

Modify an existing finish passes item

Signature Modify(index, numberOfPasses, increment)

Parameters:
  • index (int) – the index of modified item
  • numberOfPasses (int) – the number of passes
  • increment (float) – the increment

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)