TurnRoughFinishTestCutStockModeTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishTestCut.StockModeTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutStockModeTypes
-
class
NXOpen.CAM.
TurnRoughFinishTestCutStockModeTypes
¶ Bases:
object
the test cut stock mode options
Enum Members
Enum Member Enum Member Description Automatic Test Cut Stock Mode: Automatic Specify Test Cut Stock Mode: Specify SameAsFirstTestCut Test Cut Stock Mode: Same as First Test Cut -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-