TurnRoughFinishTestCutSecondarySequenceTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishTestCut.SecondarySequenceTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutSecondarySequenceTypes
-
class
NXOpen.CAM.
TurnRoughFinishTestCutSecondarySequenceTypes
¶ Bases:
object
the secondary test cut sequence options
Enum Members
Enum Member Enum Member Description NotSet Secondary Test Cut Sequence: None Diameter Secondary Test Cut Sequence: Diameter Face Secondary Test Cut Sequence: Face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-