TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishLocalReturnBuilder.ReturnMoveModeTypes is an alias for NXOpen.CAM.TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes
-
class
NXOpen.CAM.
TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes
¶ Bases:
object
the return move mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet Return Move: Nove Direct Return Move: Direct RadialAxial Return Move: Radial-Axial AxialRadial Return Move: Axial-Radial ClearRadialDirect Return Move: Clear Radial-Direct ClearAxialDirect Return Move: Clear Axial-Direct ClearRadial Return Move: Clear Radial ClearAxial Return Move: Clear Axial RadialClearAxialDirect Return Move: Radial-Clear Axial-Direct RadialAxialRadial Return Move: Radial-Axial-Radial RadialClearAxial Return Move: Radial-Clear Axial ClearRadialClearAxialDirect Return Move: Clear Radial-Clear Axial-Direct ClearRadialAxialRadial Return Move: Clear Radial-Axial-Radial ClearRadialClearAxial Return Move: Clear Radial-Clear Axial SameAsDeparture Return Move: Same as Departure. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-