TurnProbeClearanceBuilderAxialPlaneModes Enumeration¶
NXOpen.CAM.TurnProbeClearanceBuilder.AxialPlaneModes is an alias for NXOpen.CAM.TurnProbeClearanceBuilderAxialPlaneModes
-
class
NXOpen.CAM.
TurnProbeClearanceBuilderAxialPlaneModes
¶ Bases:
object
The axial plane mode options
New in version NX8.5.1.
Enum Members
Enum Member Enum Member Description NotSet Plane is inactive. Point Plane is defined by point. Distance Plane is defined by distance value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-