TurnOrientWcsXcMappingTypes Enumeration¶
NXOpen.CAM.TurnOrientWcs.XcMappingTypes is an alias for NXOpen.CAM.TurnOrientWcsXcMappingTypes
-
class
NXOpen.CAM.
TurnOrientWcsXcMappingTypes
¶ Bases:
object
the XC mapping types
Enum Members
Enum Member Enum Member Description SpindleAxis Map XC to ZM or XM of the MCS ReversedSpindleAxis Map XC to -ZM or -XM of the MCS RadialAxis Map XC to XM or YM of the MCS ReversedRadialAxis Map XC to -XM or -YM of the MCS -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-