TurnFeatureGeomBuilderSurfaceSensitivityModes Enumeration¶
NXOpen.CAM.TurnFeatureGeomBuilder.SurfaceSensitivityModes is an alias for NXOpen.CAM.TurnFeatureGeomBuilderSurfaceSensitivityModes
-
class
NXOpen.CAM.
TurnFeatureGeomBuilderSurfaceSensitivityModes
¶ Bases:
object
the surface sensitivity options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet Surface sensitivity is inactive. Distance Surface sensitivity is active. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-