TurnEngageRetractBuilderTypes Enumeration¶
NXOpen.CAM.TurnEngageRetractBuilder.Types is an alias for NXOpen.CAM.TurnEngageRetractBuilderTypes
-
class
NXOpen.CAM.
TurnEngageRetractBuilderTypes
¶ Bases:
object
The engage retract type
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description AutoCircular Auto Circular AutoLinear Auto Linear Delta Delta AngleAndDistance Angle and Distance RelativeLinear Relative Linear FromAPoint From a Point TwoCircles Two Circles TwoPointTangent Two Point Tangent SameAsEngage Same as Engage -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-