TurnEngageRetractBuilderAutoOptions Enumeration¶
NXOpen.CAM.TurnEngageRetractBuilder.AutoOptions is an alias for NXOpen.CAM.TurnEngageRetractBuilderAutoOptions
-
class
NXOpen.CAM.
TurnEngageRetractBuilderAutoOptions
¶ Bases:
object
The auto engage retract options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description UserDefinedValues User Defined Values AutomaticValues Automatic Values ClearWallsByAngleAndDistance Clear Walls by Angle and Distance Withdraw Withdraw WithdrawByDistance Withdraw by Distance ClearWalls Clear Walls ClearWallsByDistance Clear Walls by Distance SameAsPlungeRetract Same as Plunge Retract -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-