TurnConcaveCornerControlTypes Enumeration¶
NXOpen.CAM.TurnConcaveCornerControl.Types is an alias for NXOpen.CAM.TurnConcaveCornerControlTypes
-
class
NXOpen.CAM.
TurnConcaveCornerControlTypes
¶ Bases:
object
the Concave Corner Control types
New in version NX6.0.2.
Enum Members
Enum Member Enum Member Description ExtendTangents Concave Corner Control Type is Extend. Round Concave Corner Control Type is Round. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-