TurnConcaveCornerControlRadiusOptions Enumeration¶
NXOpen.CAM.TurnConcaveCornerControl.RadiusOptions is an alias for NXOpen.CAM.TurnConcaveCornerControlRadiusOptions
-
class
NXOpen.CAM.
TurnConcaveCornerControlRadiusOptions
¶ Bases:
object
the Concave Corner Control radius options
New in version NX6.0.2.
Enum Members
Enum Member Enum Member Description Specify Concave Corner Control radius option is Specify. ToolRadius Concave Corner Control radius option is Tool Radius. AddToToolRadius Concave Corner Control radius option is Add to Tool Radius. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-