TurnAvoidanceStartBuilderStartPointModes Enumeration¶
NXOpen.CAM.TurnAvoidanceStartBuilder.StartPointModes is an alias for NXOpen.CAM.TurnAvoidanceStartBuilderStartPointModes
-
class
NXOpen.CAM.
TurnAvoidanceStartBuilderStartPointModes
¶ Bases:
object
the start point mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Point Point is defined by point. DeltaAngleDistance Point is defined by angle and distance. DeltaVectorDistance Point is defined by vector and distance. DeltaMove Point is defined by delta move (X and Y coordinate). -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-