TurnAvoidancePathPointsBuilderFeedrateModesTypes Enumeration¶
NXOpen.CAM.TurnAvoidancePathPointsBuilder.FeedrateModesTypes is an alias for NXOpen.CAM.TurnAvoidancePathPointsBuilderFeedrateModesTypes
-
class
NXOpen.CAM.
TurnAvoidancePathPointsBuilderFeedrateModesTypes
¶ Bases:
object
the feed rate type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Rapid Feed Rate: Automatic ApproachOrDepature Feed Rate: Direct EngageOrReturn Feed Rate: Radial then Axial Cut Feed Rate: Axial then Radial Custom Feed Rate: Axial then Radial -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-