TurnAvoidanceGohomeBuilderGohomePointMotionTypes Enumeration¶
NXOpen.CAM.TurnAvoidanceGohomeBuilder.GohomePointMotionTypes is an alias for NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointMotionTypes
-
class
NXOpen.CAM.
TurnAvoidanceGohomeBuilderGohomePointMotionTypes
¶ Bases:
object
The gohome point motion type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet Point is inactive. Direct Motion type: Direct to point. RadialThenAxial Motion type: Radial then axial to point. AxialThenRadial Motion type: Axial then axial to point. ClearRadialThenDirect Motion type: Radial to clearance plane then direct to point. ClearAxialThenDirect Motion type: Axial to clearance plane then direct to point. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-