TrimPlane Class¶
-
class
NXOpen.CAM.
TrimPlane
¶ Bases:
NXOpen.TaggedObject
Represents Trim Plane
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
LimitOption | Returns or sets the limit option |
Point | Returns or sets the trim plane point |
Radius | Returns the radius |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TrimPlaneContent Enumeration | The content options |
TrimPlaneLimitOptions Enumeration | The limit options |
Property Detail¶
LimitOption¶
-
TrimPlane.
LimitOption
¶ Returns or sets the limit option
-------------------------------------
Getter Method
Signature
LimitOption
Returns: the limit option Return type: NXOpen.CAM.TrimPlaneLimitOptions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitOption
Parameters: trimPlaneMode ( NXOpen.CAM.TrimPlaneLimitOptions
) – the limit optionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
TrimPlane.
Point
¶ Returns or sets the trim plane point
-------------------------------------
Getter Method
Signature
Point
Returns: the trim plane point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) – the trim plane pointNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Radius¶
-
TrimPlane.
Radius
¶ Returns the radius
-------------------------------------
Getter Method
Signature
Radius
Returns: the Radius Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.