Topology Class¶
-
class
NXOpen.CAM.
Topology
¶ Bases:
NXOpen.Builder
Represents a CAM topology builder
Use the
NXOpen.CAM.Geometry
class to get a topology builderNew in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
DistanceTolerance | Returns or sets the distance tolerance |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetShellCount | Get the count of shell anchors |
Rebuild | The action of rebuild topology data |
RemoveShell | Remove shell set |
ReverseMaterialSide | The action of reverse material side of one connected shell |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnifyMaterialSide | The action of unify material side of one connected shell |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
Topology.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: the angle tolerance Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: newValue (float) – the angle tolerance New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
DistanceTolerance¶
-
Topology.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: the distance tolerance Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: newValue (float) – the distance tolerance New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetShellCount¶
-
Topology.
GetShellCount
¶ Get the count of shell anchors
Signature
GetShellCount()
Returns: Return type: int New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Rebuild¶
-
Topology.
Rebuild
¶ The action of rebuild topology data
Signature
Rebuild()
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
RemoveShell¶
-
Topology.
RemoveShell
¶ Remove shell set
Signature
RemoveShell(shellIndex)
Parameters: shellIndex (int) – the index of shell anchor New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ReverseMaterialSide¶
-
Topology.
ReverseMaterialSide
¶ The action of reverse material side of one connected shell
Signature
ReverseMaterialSide(shellIndex)
Parameters: shellIndex (int) – the index of shell anchor New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
UnifyMaterialSide¶
-
Topology.
UnifyMaterialSide
¶ The action of unify material side of one connected shell
Signature
UnifyMaterialSide(shellIndex)
Parameters: shellIndex (int) – the index of shell anchor New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
Topology.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.