ToolTypes Enumeration¶
NXOpen.CAM.Tool.Types is an alias for NXOpen.CAM.ToolTypes
-
class
NXOpen.CAM.
ToolTypes
¶ Bases:
object
Tool types
Enum Members
Enum Member Enum Member Description Mill Milling tool Drill Drilling tool Turn Turning tool Groove Grooving tool Thread Threading tool Wedm WEDM tool Barrel Milling tool-Barrel Tcutter Milling tool-T cutter Form Form tool DrillSpcGroove Milling tool-T cutter Solid Solid tool MillForm User defined mill tool Laser laser tool Soft -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-