ToolSubtypes Enumeration¶
NXOpen.CAM.Tool.Subtypes is an alias for NXOpen.CAM.ToolSubtypes
-
class
NXOpen.CAM.
ToolSubtypes
¶ Bases:
object
Tool subtypes
Enum Members
Enum Member Enum Member Description Undefined Mill5 Milling tool-5 parameters Mill7 Milling tool-7 parameters Mill10 Milling tool-10 parameters MillBall Milling tool-Ball mill DrillStandard Drilling tool DrillCenterBell Centerdrill DrillCountersink Countersink DrillSpotFace Spot facing tool DrillSpotDrill Spot drill DrillBore Boring tool DrillReam Reamer DrillCounterbore Counterbore DrillTap Tap DrillBurnishing Burnishing tool DrillThreadMill Thread mill DrillBackSpotFace Back spot facing tool DrillStep Step drill TurnStandard Turning tool-Standard TurnButton Turning tool-Button TurnBoringBar Turning tool-Boring bar GrooveStandard Grooving tool-Standard GrooveRing Grooving tool-Ring GrooveFullNoseRadius Grooving tool-Full nose radius GrooveUserDefined Grooving tool-User defined ThreadStandard Threading tool-Standard ThreadButress Threading tool-Butress ThreadAcme Threading tool-ACME ThreadTrapezoidal Threading tool-Trapezoidal Generic Solid tool generic Probe Probe MillChamfer Milling chamfer mill MillSpherical Milling spherical mill DrillCore Core Drill StdLaser Standard Laser tool Laser DrillBackCountersink Back Countersink CoaxialLaser Coaxial Laser tool DrillBoringBar Boring Bar tool DrillChamferBoringBar Chamfer Boring Bar tool -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-