ToolPathTiltTiltingToolAxisTypes Enumeration¶
NXOpen.CAM.ToolPathTiltTilting.ToolAxisTypes is an alias for NXOpen.CAM.ToolPathTiltTiltingToolAxisTypes
-
class
NXOpen.CAM.
ToolPathTiltTiltingToolAxisTypes
¶ Bases:
object
the tool axis mode options
Enum Members
Enum Member Enum Member Description TowardCurve Tool axis mode: towards curve FromCurve Tool axis mode: from curve TowardPoint Tool axis mode: towards point FromPoint Tool axis mode: from point RelativeAngle Tool axis mode: relative MCS -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-