ToolPathTiltTiltingToolAxisTiltingRuleTypes Enumeration¶
NXOpen.CAM.ToolPathTiltTilting.ToolAxisTiltingRuleTypes is an alias for NXOpen.CAM.ToolPathTiltTiltingToolAxisTiltingRuleTypes
-
class
NXOpen.CAM.
ToolPathTiltTiltingToolAxisTiltingRuleTypes
¶ Bases:
object
the tool tilting rule options
Enum Members
Enum Member Enum Member Description MainDir Tool tilting rule main direction AwayFrom Tool tilting rule away from TowardConst Tool tilting rule toward constant Through Tool tilting rule through -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-