ToolPathTiltTiltingManualTiltTypes Enumeration

NXOpen.CAM.ToolPathTiltTilting.ManualTiltTypes is an alias for NXOpen.CAM.ToolPathTiltTiltingManualTiltTypes

class NXOpen.CAM.ToolPathTiltTiltingManualTiltTypes

Bases: object

the manual tilt

Enum Members

Enum Member Enum Member Description
KeepOriginal
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.