ToolPathEditorBuilderTrimGeometryType Enumeration

NXOpen.CAM.ToolPathEditorBuilder.TrimGeometryType is an alias for NXOpen.CAM.ToolPathEditorBuilderTrimGeometryType

class NXOpen.CAM.ToolPathEditorBuilderTrimGeometryType

Bases: object

Trim Geometry Type

Enum Members

Enum Member Enum Member Description
Plane
LineInView
Boundary
PermanentBoundary
SelectionInView
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.