ToolPathEditorBuilderExtendMethodType Enumeration

NXOpen.CAM.ToolPathEditorBuilder.ExtendMethodType is an alias for NXOpen.CAM.ToolPathEditorBuilderExtendMethodType

class NXOpen.CAM.ToolPathEditorBuilderExtendMethodType

Bases: object

Extend Method Type

Enum Members

Enum Member Enum Member Description
Linear
Arc
LinearArc
ArcLinear
LinearArcLinear
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.