ToolPathEditorBuilderConnectionMethodType Enumeration

NXOpen.CAM.ToolPathEditorBuilder.ConnectionMethodType is an alias for NXOpen.CAM.ToolPathEditorBuilderConnectionMethodType

class NXOpen.CAM.ToolPathEditorBuilderConnectionMethodType

Bases: object

Connection Method Type

Enum Members

Enum Member Enum Member Description
ClearancePlane
Direct
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.