ToolAxisVariableTypes Enumeration¶
NXOpen.CAM.ToolAxisVariable.Types is an alias for NXOpen.CAM.ToolAxisVariableTypes
-
class
NXOpen.CAM.
ToolAxisVariableTypes
¶ Bases:
object
Available types for Tool Axis Variable
Enum Members
Enum Member Enum Member Description AwayFromPoint Away from Point TowardPoint Toward Point AwayFromLine Away from Line TowardLine Toward Line RelativeToVector Relative to Vector NormalToPart Normal to Part RelativeToPart Relative to Part FourAxisNormalToPart 4-Axis Normal to Part FourAxisRelativeToPart 4-Axis Relative to Part DualFourAxisOnPart Dual 4-Axis on Part InterpolateVector Interpolate Vector InterpolateAngleToPart Interpolate Angle to Part InterpolateAngleToDrive Interpolate Angle to Drive OptimizedToDrive Optimized to Drive NormalToDrive Normal to Drive SwarfDrive Swarf Drive RelativeToDrive Relative to Drive FourAxisNormalToDrive 4-Axis Normal to Drive FourAxisRelativeToDrive 4-Axis Relative to Drive DualFourAxisOnDrive Dual 4-Axis on Drive SameAsDrivePath Same as drive path UserDefined User Defined Automatic Original VAP tool axis AlignToEdges Align to almost straight edges SwarfBaseUV Align to U or V parameter line FourAxisAroundRotaryAxis 4-Axis Around Rotary Axis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-