ToolAxisTiltTypes Enumeration¶
NXOpen.CAM.ToolAxisTilt.Types is an alias for NXOpen.CAM.ToolAxisTiltTypes
-
class
NXOpen.CAM.
ToolAxisTiltTypes
¶ Bases:
object
Available types for tool axis tilt control
Enum Members
Enum Member Enum Member Description NotSet No tilting AwayFromPart Tilt away from part AwayFromPoint Tilt away from point TowardPoint Tilt tpward point AwayFromCurve Tilt away from curve TowardCurve Tilt toward curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-