ToolAxisInterpolateInterpolateTypes Enumeration¶
NXOpen.CAM.ToolAxisInterpolate.InterpolateTypes is an alias for NXOpen.CAM.ToolAxisInterpolateInterpolateTypes
-
class
NXOpen.CAM.
ToolAxisInterpolateInterpolateTypes
¶ Bases:
object
the available types for Interpolate Types
Enum Members
Enum Member Enum Member Description Vector Interpolate Types: Vector AngleToPart Interpolate Types: Angle to Part AngleToDrive Interpolate Types: Angle to Drive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-