ToolAxisChangeMethodTypes Enumeration

NXOpen.CAM.ToolAxisChange.MethodTypes is an alias for NXOpen.CAM.ToolAxisChangeMethodTypes

class NXOpen.CAM.ToolAxisChangeMethodTypes

Bases: object

Available types for tool axis change method

Enum Members

Enum Member Enum Member Description
PerStep Per Step
PerMinute Per Minute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.